AIN#.DEADBANDMODE

Description

When AIN#.DEADBANDMODE is set to 0, and the value of the analog input is less than the absolute value of AIN#.DEADBAND, the analog command will be 0. When the analog input is greater or equal to the absolute value of AIN#.DEADBAND, then the analog command will be generated using the scaling specified.

When AIN#.DEADBANDMODE is set to 1, the analog command is 0 if the input is less than the absolute value of the deadband value. When the input is greater than the absolute value of the deadband, the output is equal to (Input - Deadband) * Scaling.

Below are illustrations of this behavior.

Examples

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  
Stored in Non-Volatile Memory Yes
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
AIN1.DEADBANDMODE

3780h

03h

Unsigned16

-

-

Read/Write

No

AIN2.DEADBANDMODE

3781h

03h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AIN1.DEADBANDMODE

23200

5AA0

Unsigned16

Read/Write

-

AIN2.DEADBANDMODE

23201

5AA1

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AIN1.DEADBANDMODE

23200

Unsigned16

Read/Write

-

AIN2.DEADBANDMODE

23201

Unsigned16

Read/Write

-